2013-01-26 1:36 PM
Is there a place that one can get the pinout tables for the STM32 family devices in a format other than PDF? The tables in the PDF datasheets and reference manuals are not easily copied to other software, and it seems cumbersome and mistake-prone to have to copy the tables by hand into a tool like excel or a text editor.
Particularly, I'm interested in the pinout table for the STM32F0 devices, but if there's a place we can go to get this for any device, that would be awesome. #pinout-spreadsheet-pdf-textfile2013-01-28 12:32 AM
I have the 'F4xx pinout table reworked into OOo Calc format (which can be converted to Excel or whatever else), as in http://www.efton.sk/STM32/STM32F4xx%20misc.pdf .
There are some xml files available with the MicroXplorer soft, but it may be not trivial to rework them into anything usable. JW