cancel
Showing results for 
Search instead for 
Did you mean: 

Data transfer between two STM32 devices using FSMC

tecnico23
Associate II
Posted on January 26, 2013 at 22:45

Hi,

I'm currious if it is possible to share data between two STM32 devices, using the FSMC interface.

Is it possible to configure one device as a Master and the other as a slave and use the FSMC? I would make the slave device act, as it was a SRAM memory, for example.

If not, is there a parallel peripheral to transfer data between two STM32 devices?

Thanks in advance,

Regards,

A. Paiva
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on January 27, 2013 at 02:02

Not really, it's an outbound interface, and there isn't a way to do a DMA type REQ/ACK protocol externally. Synchronization was also be an issue.

The best way to attack this would be using a dual-port memory or FIFO, or use an FPGA
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on January 28, 2013 at 09:12

Maybe the camera interface could be used as a slave, but it's surely not an out-of-the-box solution.

JW

tecnico23
Associate II
Posted on January 28, 2013 at 10:14

Ok,

Thank you all!

Regards

A. Paiva