2018-04-30 3:57 AM
I am trying to digitally turn LED HIGH and LOW using STM32F103C8T6 maple mini board using pins A11, A12, B4 and A15 pin, But it seems that those pins are internally pulled up as soon as I power it on stm32 boards this pins get +3.3, 1.9 and 0.5 volt, If this pins are internally pulled up, How do I make them work? and If i try to digitally turn those pins HIGH and LOW using programming, this does not bring any effect on LED's. I would like to know, How do i control LED's using these pins,
Regards
Anurag Mahajan
2018-05-01 12:59 AM
PA11 and PA12 are USB DM and USB DP. Don't you have USB connected?
Similarly, check what's connected to the remaining pins on the board. They may be used by the debugging header (JTAG or SWD), if there is one.
JW