2023-01-12 11:57 PM
Hi!
I am working with a STM32L053 MCU. I would like to write to the internal eeprom, and based on the datasheet it takes 3.2 ms.
I have doubts that during that time interrupts will be ignored. It is not clear for me why.
I thought that the code is in the flash and the eeprom is independent from the flash.
(Or maybe this EEPROM is not a real EEPROM, but emulated EEPROM in flash?)
Best regards
2023-01-13 5:57 AM
Hello @Attila Szabo (Community Member)
I can suggest the recommendation of AN4808 for STM32L0.
And firmware packege X-CUBE-NVMRWW.
https://www.st.com/en/embedded-software/x-cube-nvmrww.html
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.