Skip to main content
NASI
Associate III
January 11, 2023
Question

Jump To Application From

  • January 11, 2023
  • 19 replies
  • 7636 views

Hello,

I am working on a custom bootloader for STM32F105 which it is possible to write a bin file into the flash via CAN bus(CAN2).

My issue is that the part of bootloader to jump to application doesn't work.

Here is the jump function code:

#define MAIN_PROGRAM_START_ADDRESS 0x08002000
 
void JumpToApplication(void)
{
 JumpAddress = *(__IO uint32_t*)(MAIN_PROGRAM_START_ADDRESS + 4);
 Jump_To_Application = (pFunction) JumpAddress;
 
 __HAL_RCC_GPIOC_CLK_DISABLE();
 __HAL_RCC_GPIOD_CLK_DISABLE();
 __HAL_RCC_GPIOB_CLK_DISABLE();
 __HAL_RCC_GPIOA_CLK_DISABLE();
	HAL_RCC_DeInit();
	HAL_DeInit();
	SysTick->CTRL = 0;
	SysTick->LOAD = 0;
	SysTick->VAL = 0;
 
 /**
 * Step: Disable all interrupts
 */
 __disable_irq();
 
 __set_MSP(*(volatile uint32_t*) MAIN_PROGRAM_START_ADDRESS);
 
 Jump_To_Application();
}

Function HAL_RCC_DeInit() jumps directly to HardFault_Handler(). I am using an external crystal ocsilator 8MHz.

Without calling HAL_RCC_DeInit(), the Jump_To_Application() jumps directly to HardFault_Handler().

Any idea?

Thank you.

This topic has been closed for replies.

19 replies

Javier1
Principal
January 11, 2023

Hi @NASI​ , i just developed the same thing last year.

Canbus Bootloader for stm32f105 families, it has been working for some time now.

This is my jump to app function:

void jumpToApp(const uint32_t address) {
	const JumpStruct *vector_p = (JumpStruct*) address;
 
	deinitEverything();
 
	/* let's do The Jump! */
	/* Jump, used asm to avoid stack optimization */
	asm("msr msp, %0; bx %1;" : : "r"(vector_p->stack_addr), "r"(vector_p->func_p));
}
void deinitEverything() {
	//-- reset peripherals to guarantee flawless start of user application
	//	HAL_GPIO_DeInit(LED_GPIO_Port, LED_Pin);
	HAL_GPIO_DeInit(CAN1_TX_BOOTLOADER_GPIO_Port, CAN1_TX_BOOTLOADER_Pin);
	HAL_GPIO_DeInit(CAN1_RX_BOOTLOADER_GPIO_Port, CAN1_RX_BOOTLOADER_Pin);
	HAL_CAN_DeInit(_hcan);
	HAL_RCC_DeInit();
	HAL_DeInit();
	SysTick->CTRL = 0;
	SysTick->LOAD = 0;
	SysTick->VAL = 0;
}
/////////////////////////////////////////////////////blind jump to memory struct
typedef void (application_t)(void);
 
typedef struct
{
 uint32_t		stack_addr; // Stack Pointer
 application_t*	func_p; // Program Counter
} JumpStruct;
//////////////////////////////////////////////////////

 >> I am using an external crystal ocsilator 8MHz.

Gooooood! i didnt and i suffered great deal

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

Hi @Javier Muñoz​ ,

I am using also almost the same functions, but calling the HAL_RCC_DeInit() goes wrong, jumps to HardFault_Handler().

Javier1
Principal
January 11, 2023

did you debugged line by line? (inside HAL_RCC_deinit)

extra idea, are you calling JumpToApplication inside an IRQ? because if you are the systick might be frozen.0693W00000Y7yPaQAJ.png

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

Yes, I did:

HAL_StatusTypeDef HAL_RCC_DeInit(void)
{
 uint32_t tickstart;
 
 /* Get Start Tick */
 tickstart = HAL_GetTick();
 
 /* Set HSION bit */
 SET_BIT(RCC->CR, RCC_CR_HSION);
 
 /* Wait till HSI is ready */
 while (READ_BIT(RCC->CR, RCC_CR_HSIRDY) == RESET)
 {
 if ((HAL_GetTick() - tickstart) > HSI_TIMEOUT_VALUE)
 {
 return HAL_TIMEOUT;
 }
 }
......

The first line "tickstart = HAL_GetTick();" jumps to fault handler

Javier1
Principal
January 11, 2023

somthing fishy is going on with your systick

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

No, I am calling JumpToApplication from main().

Javier1
Principal
January 11, 2023

place a HAL_Delay(100): in main does it fail also?

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

Yes, It does

Javier1
Principal
January 11, 2023

there you have the culprit, show me how youre initialicing the systick

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Principal
January 11, 2023

show me this bit from your code0693W00000Y7yZGQAZ.png

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

Here:

0693W00000Y7ybMQAR.png

Javier1
Principal
January 11, 2023

looks alright, is the systick ticking at all?

Take a look at "uwTick" variable in your live expressions while debugging

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

Yes the variable is ticking

Javier1
Principal
January 11, 2023

Thats weird because

>>The first line "tickstart = HAL_GetTick();" jumps to fault handler

HAL_GetTick just returns that variable

__weak uint32_t HAL_GetTick(void)
{
 return uwTick;
}

If i were you i would start all over again fresh CubeMX project, only the XTAL and make sure hal_delay is working , keep adding stuff untill it breaks again.

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 11, 2023

Now the second line SET_BIT(RCC->CR, RCC_CR_HSION) jumps to fault handler.

NASI
NASIAuthor
Associate III
January 12, 2023

I made .ioc file for bootloader as the same as .ioc file for the application, and HAL_RCC_deinit() didn't jump to hard fault.

But the last line of the jump function Jump_To_Application() jumps now to hard fault interrupt.

0693W00000Y85TtQAJ.png 

NASI
NASIAuthor
Associate III
January 13, 2023

I have fixed the issue and the bootloader works fine.

Javier1
Principal
January 13, 2023

Congratulations, do you mind explaining how for the next person that has a similar problem?

hit me up in https://www.linkedin.com/in/javiermuñoz/
NASI
NASIAuthor
Associate III
January 13, 2023

As I mentioned I fixed the hard fault issue by using the same ioc file for bootloader as application (just initialization) and then I found that I didn't program data correctly on the flash.

Now I am able to jump to application, but after I make a power cycle (reset) on PCB, the application doesn't start anymore. So, I am still working on it.