Skip to main content
Associate
November 19, 2024
Question

STM32 G4 HAL i2c not clearing interrupts

  • November 19, 2024
  • 3 replies
  • 1556 views
**Problem:**

- When the I2C is enabled, the part can hit the WWDG.
- It looks like the pointer to the function `XferISR` is getting set to NULL somehow.
  - When this happens, the interrupts are not cleared, and it continually fires the interrupt because it is never cleared.
  - This is hard to troubleshoot because, in my system, there are many higher priority interrupts, making it hard to know that this is the problem.
- On another note, it looks like the interrupts are not always cleared in accordance with **RM0440 Table 394**:
  - In the error section, I2C_FLAG_PECERR, I2C_FLAG_TIMEOUT, and I2C_FLAG_ALERT are never cleared.
  - Also in I2C_Master_ISR_IT.

**Background:**

- Using an STM32G4 with HAL v1.2.3.
- Using DMA or IT (different builds).
- Connected to many I2C sensors.
- It is in a pretty noisy environment.
- All calls are from the main loop (except what was generated by HAL); all reading of buffers is in the main loop.
- If I have an I2C error, I re-init the I2C to clear out problems.

**Recommended Solutions:**

```c
void HAL_I2C_EV_IRQHandler(I2C_HandleTypeDef *hi2c) /* Derogation MISRAC2012-Rule-8.13 */
{
  /* Get current IT Flags and IT sources value */
  uint32_t itflags   = READ_REG(hi2c->Instance->ISR);
  uint32_t itsources = READ_REG(hi2c->Instance->CR1);

  /* I2C events treatment -------------------------------------*/
  if (hi2c->XferISR != NULL)
  {
    hi2c->XferISR(hi2c, itflags, itsources);
  }
  /* Add this */
  else
  {
    /* if you are very confident in the HAL */
    ASSERT();
    /* else */
    ClearAllI2cInterrupts(hi2c);
  }
  /* End Add */
}
```

- When there is a problem, you want to bring that to the attention of the developer to deal with it.
- I would think clearing all I2C interrupts would be more palatable.
- Also, where `XferISR = NULL`, you could set `XferISR = ClearAllI2cInterrupts;` this way, it better covers the bases.

**Questions:**

- Have you seen `XferISR` set to NULL while getting interrupts?
- Do you have any ideas why this might happen?

**Final Remarks:**

- I am going to try this out. Maybe I am smashing memory and setting `XferISR = NULL`. If after initialization it should never be NULL and then it got set to NULL, then likely I did something wrong...
This topic has been closed for replies.

3 replies

ST Technical Moderator
January 7, 2025

Hello @photon 

These flags "I2C_FLAG_PECERR, I2C_FLAG_TIMEOUT, and I2C_FLAG_ALERT" cannot be cleared by software. They are cleared by hardware when disabling the peripheral. 

Saket_Om_0-1736258746594.png 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
photonAuthor
Associate
January 7, 2025

More background

  • There is high amounts of high priority interrupts happening in this system (that you don't see)
  • Here are some of my interrupt priorities:

 

#define NVIC_PRI_WWDG (1UL)
#define NVIC_PRI_PWR (1UL)
...
#define NVIC_PRI_SYS_TICK (3UL)
#define NVIC_PRI_EXTI (4UL)
#define NVIC_PRI_DMA_I2C_RX (4UL)
#define NVIC_PRI_DMA_I2C_TX (4UL)
#define NVIC_PRI_DMA_I2C_RXERR (4UL)
#define NVIC_PRI_I2C2_EV_IRQn (11UL)
#define NVIC_PRI_I2C2_ER_IRQn (11UL)

 

Further investigation and fixes

Potential thread safety violation

  • Compare function pointer to NULL then call it, but it could have been changed between the check and the call.
  • This can be fixed by creating a local variable that grabs the value compares that value then calls the stored value.
  • Was:

 

void HAL_I2C_EV_IRQHandler(I2C_HandleTypeDef *hi2c) /* Derogation MISRAC2012-Rule-8.13 */
{
 /* Get current IT Flags and IT sources value */
 uint32_t itflags = READ_REG(hi2c->Instance->ISR);
 uint32_t itsources = READ_REG(hi2c->Instance->CR1);

 /* I2C events treatment -------------------------------------*/
 if (hi2c->XferISR != NULL)
 {
 hi2c->XferISR(hi2c, itflags, itsources);
 }
}

 

  • Fix:

 

void HAL_I2C_EV_IRQHandler(I2C_HandleTypeDef *hi2c) /* Derogation MISRAC2012-Rule-8.13 */
{
 /* Get current IT Flags and IT sources value */
 uint32_t itflags = READ_REG(hi2c->Instance->ISR);
 uint32_t itsources = READ_REG(hi2c->Instance->CR1);
 HAL_StatusTypeDef(*pFoo)(struct __I2C_HandleTypeDef *hi2c, uint32_t ITFlags, uint32_t ITSources);
 pFoo = hi2c->XferISR;

 /* I2C events treatment -------------------------------------*/
 if (NULL != pFoo)
 {
 pFoo(hi2c, itflags & I2C_EV_MASK_IT, itsources);
 }
}

 

 

Create a pointer to function will clear un-expected interrupts

 

#define I2C_EV_MASK_IT ( I2C_FLAG_TXE | I2C_FLAG_TXIS | I2C_FLAG_RXNE | I2C_FLAG_ADDR \
 | I2C_FLAG_AF | I2C_FLAG_STOPF | I2C_FLAG_TC | I2C_FLAG_TCR )
#define I2C_ER_MASK_IT ( I2C_FLAG_BERR | I2C_FLAG_ARLO | I2C_FLAG_OVR \
 | I2C_FLAG_PECERR | I2C_FLAG_TIMEOUT | I2C_FLAG_ALERT )

HAL_StatusTypeDef I2C_Null_IT(struct __I2C_HandleTypeDef *hi2c, uint32_t ITFlags,
 uint32_t ITSources)
{
 __HAL_LOCK(hi2c);

 /* Disable interupts */
 __HAL_I2C_DISABLE_IT(hi2c, ITFlags & (I2C_EV_MASK_IT | I2C_ER_MASK_IT ));
 __HAL_I2C_CLEAR_FLAG(hi2c, ITFlags & (I2C_EV_MASK_IT | I2C_ER_MASK_IT ));

 __HAL_UNLOCK(hi2c);
 return (HAL_OK);
}

 

  • Changes
    • Was: hi2c->XferISR = NULL;
    • Fix: hi2c->XferISR = I2C_Null_IT;
    • Change applied to
      • static void I2C_ITMasterSeqCplt(I2C_HandleTypeDef *hi2c)
      • static void I2C_ITMasterCplt(I2C_HandleTypeDef *hi2c, uint32_t ITFlags)
      • static void I2C_ITError(I2C_HandleTypeDef *hi2c, uint32_t ErrorCode)
      • Likely should be done in all the i2c interrupt functions.

Where I stand now

  • I have not determined all the changes are needed. As I never set XferISR back to NULL doesn't allow for the opportunity to create a thead safety violation.
    • Fixing the thead safety seems important and I would recommend should be done for keeping good practices.
    • Fixing thead safety alone might not be enough to prevent a lockup.
  • These change seem to mitigate the WWDG from firing because i2c interrupts locking up.
  • I do not accept your solution as a fix, as it does not fix anything.
    • Pointing out that you don't need to clear these errors does change the fact that the i2c library was hanging in an interrupt when XferISR was set to NULL.
    • Making it not able to clear the interrupt
    • The interrupt continue to fire causing starving of the main loop
    • Creating a WWDG event
  • Possible "Accept as Solution" include fixing my lockup problem that could include:
    • Explain how to use HAL so I don't get that problem.
    • Change the HAL so I don't get this problem.
ST Technical Moderator
January 9, 2025

Hello @photon 

For the moment, it is up to the user to manage the race condition on HAL access. This can be done using a software semaphore. By implementing a software semaphore, you can control access to the HAL, ensuring that only one process or thread can access it at a time, thus preventing race conditions.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om