cancel
Showing results for 
Search instead for 
Did you mean: 

An odd difference between homologous functions in hal_uart vs hal_usart.

elKarro
Associate III

Hi, any idea about why stm32xx_hal_uart functions write to USART control registers by ATOMIC_CLEAR_BIT()/ATOMIC_SET_BIT(), while homologous stm32xx_hal_usart functions write to the same registers by CLEAR_BIT()/SET_BIT()?

In example:
UART_DMATransmitCplt() -> ATOMIC_CLEAR_BIT(huart ->Instance->CR3, USART_CR3_DMAT);
USART_DMATransmitCplt() -> CLEAR_BIT(husart->Instance->CR3, USART_CR3_DMAT);

Since both UART/USART are referred to by the same USART_TypeDef structure, I'd be expected to use them in the same way. So, is that due to some undocumented difference in the silicon between UART/USART?

MCU speaks VHDL and CPU speaks assembly. Neither of them speaks HAL.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

'By convention' (or 'historic reasons') the HAL based code uses stm32xx_hal_uart module for both USART and UART IPs, for the most common async mode. So it looks that the stm32xx_hal_usart module is neglected. Do you think you have a genuine need for the "uart" module?

 

View solution in original post

7 REPLIES 7
TDK
Super User

UART is asynchronous in the sense that RX and TX can be happening at the same time, independently of each other. If using DMA, the TX interrupt could pre-empt the RX interrupt if you have them set up that way. USART is not, they happen synchronously with a single clock signal. So the interrupts should not overlap each other and there is no need to make "atomic" accesses.

USART is close to SPI in terms of architecture.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Super User

'By convention' (or 'historic reasons') the HAL based code uses stm32xx_hal_uart module for both USART and UART IPs, for the most common async mode. So it looks that the stm32xx_hal_usart module is neglected. Do you think you have a genuine need for the "uart" module?

 

I think I haven't a genuine need for both, since I always write my own drivers :)
I only read HAL code to try to fill the lack of documentation and this time a neglected module adds even more chaos.

USART has a S (sync) more than UART, the peripheral struct itself is named USART_TypeDef, but stm32xx_hal_uart module is maintained while stm32xx_hal_usart is neglected?
For 'historic reasons' I see nations where they write the year in letters... the unification should be applied to the stm32xx_hal_usart module, don't you think?

"With Cube and a Nucleo, the deli worker too can build a speed controller for his slicer!"
Come on ST, less marketing and more engineering.

MCU speaks VHDL and CPU speaks assembly. Neither of them speaks HAL.

@TDK wrote:

USART is close to SPI in terms of architecture.


but only when used in the sync mode, surely?

when used in async mode, a USART is just a UART, surely?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
elKarro
Associate III

Thanks for the clarification.

MCU speaks VHDL and CPU speaks assembly. Neither of them speaks HAL.

I think I haven't a genuine need for both, since I always write my own drivers :)

This is the best :)

 

 the unification should be applied to the stm32xx_hal_usart module, don't you think?

I guess they wanted to unify USARTs and UARTs (perhaps LPUARTs too) at the HAL level, all covered by stm32xx_hal_uart module. stm32xx_hal_usart should then be dropped.  The differences should remain in the low level (LL) modules as they are closest to the register-level. The world is not ideal, may this be our worst problem.

 

 

The USART functions are only used in USART mode.

If you use the USART1 peripheral in UART mode, you are using UART functions (e.g. HAL_UART_*).

If you feel a post has answered your question, please click "Accept as Solution".