2013-10-27 08:14 PM
Hi everybody,
I'm working with OV2640 and i've problem with brightness. I use TFT LCD to display, use config from STM32F4xx_DSP_StdPeriph_Lib ( dcmi_ov2640.c). DMA and DCMI working fine but the image i receive too dark. So, i use :void OV2640_BrightnessConfig(uint8_t Brightness){ OV2640_WriteReg(0xff, 0x00); OV2640_WriteReg(0x7c, 0x00); OV2640_WriteReg(0x7d, 0x04); OV2640_WriteReg(0x7c, 0x09); OV2640_WriteReg(0x7d, Brightness); OV2640_WriteReg(0x7d, 0x00);}to increase brightness but the image still dark. I check datasheet of ov2640 for 0x7c and 0x7d reg but i can't find it. I think the config for this ov2640 is wrong, i want to correct it but they config a lot of regs that doesn't describe in the datasheet. I'm going to contact ovt for these reg setting, hope they answer...2013-10-28 06:47 AM
Not much support here for cameras. And I don't suppose OVT provides support to random users. If you're commercial push through usual distribution and FAE channels.
What does the image look like if you upload to a PC and view there? Is the lens obstructed, with tape, or something? Issues with voltages and clocks? http://lxr.free-electrons.com/source/drivers/media/video/ov2640.c?v=2.6.39[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/DCMI%20ov2640%20JPEG%2c%20not%20working&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=211]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FDCMI%20ov2640%20JPEG%2C%20not%20working&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=211