2021-07-27 2:05 AM
I have connect STM32H7xx device with Quectel MC60 GPRS Modem via UART. Instead of working with several AT commands to send the packet over SSL layer. I would like integrate with any open Cellular library which can used to enable PPPoE over Serial to send the REST packets over HTTPS protocol ?.
Any suggestions ?
2021-08-03 10:34 PM
any suggestions please ?