cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 CAN2 normal mode not working

MBRAH.1
Associate

Hello,

I have problem in CAN2 STM32F4, that in mode Loopback working good, but when

i change it to mode Normal not working (not transmission )

Please do you have a solution for working in the mode Normal ?

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

In normal mode, you should use an external CAN transceiver + another CAN node connected to the bus in order to setup a CAN communication.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
SofLit
ST Employee

Hello,

In normal mode, you should use an external CAN transceiver + another CAN node connected to the bus in order to setup a CAN communication.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.