2024-12-20 04:49 AM - last edited on 2024-12-20 04:50 AM by SofLit
Hello,
I have been trying to implement IAP in my device. But my code gets stuck in "UART_WaitOnFlagUntilTimeout". For once I was able to transfer the binary file of the new user application but later whenever I am trying to send the binary file it is getting stuck. It doesn't even show any debug error message.
I took reference from this: https://github.com/stm32-hotspot/STM32G0xx_IAP/tree/main
I have kept the IAP main at starting address which is 0x08000000 and my user application at 0x08008000.
2025-01-12 07:09 PM
did you get any progress on this issue?
Now I am also designning a IAP for STM32G474VET6, I have the same issue as you I think, when I start to transfer bin file with tera term, the transfer stopped and I step into the code, it seems UART_Receive time_out
I did this design according to AN4657. the tranfer with tera term as below
I also used uart1, I am sure it can work, because i received the menu and send 1 for choosing download.
any progress, please contact me.
thanks.
2025-01-29 09:42 PM
@dqsh06 I have tried every option possible but couldn't find the solution.
I do get the menu and it waits for the binary file when pressed 1.
2025-01-31 01:19 PM
@jowakar122 Possibly you have receive overflow. HAL_UART_Receive to receive by one byte is very inefficient and prone to RX overflows. Use a better way.
2025-02-04 06:32 PM
I have asked a chinese ST application engineer, he said he can do that, but he used uart2, do you think uart1 is different with uart2?
thanks.
2025-02-05 07:27 AM
@dqsh06 All UARTs of STM32 can have different capabilities. Please see the UARTs section in the Data Sheet (DS) document. Specific capabilities of all UARTs are described there.