2013-12-04 2:08 AM
Dear all
I have developed a USB MIDI device product based on STM32L151.Now I would like to make this product working with Apple MFi protocol.
I was wondering if I could find somewhere some inputs about MFi source code or libraries compatible with STM32 ICs.I need to add authentication processor and I'm quite sure there are some existing libraries to communicate with that authentication IC.Thanks for any tip, link, suggestion and so on !Jerome #mfi #stm32-stm32l151 #apple2018-09-24 8:13 PM
Please respond to the query . I want to develop same type of application.
2018-09-24 10:15 PM
https://developer.apple.com/programs/mfi/
Join the program, get the tools, ...
If you want someone else to develop the application I'm sure there are people who can provide consultancy.