cancel
Showing results for 
Search instead for 
Did you mean: 

STM I2C-3 not generating a clock and data signal on one of the I2Cs.

CGrov.1
Associate II

I am running an STM32L476RG at 1.8V and have noticed that I2C-3 does not generate a clock or data signal. I have tried isolating the MCU from the rest of the circuit and found that there is still no signal at the MCU pins, so i know the circuit is not loading the chip. I have changed the MCU and still get an identical signal, and I have run the circuit with an external MCU at 3.3V with no problems. Because of all this I a confident the problem is with the MCU, although I2C-1 is working perfectly. When I look at the output of the SCL3 and SDA3 with a scope, i can see the voltae rise to about 0.9V and then slowly drop back down. In comparisson, the SCL1 and SDA1 lines of the working I2C-1 rises to about 2V, and then the clock and data signals start as the voltage level drops back down.

I am wondering if it could be a product of running it at the low voltage threshold? are there any other pins (pulled high or something?) I need to worry about when using the I2C3? I can't find anything in the datasheet about this.

10 REPLIES 10
TDK
Guru

It seems very odd for a pin to get pulled up to 1.0V when the rail is at 1.8V. I'm suspicious that you have something else going on with the board that isn't mentioned.

Is the voltage on the I2C3 pins also 1.0V when NRST is low?

If you feel a post has answered your question, please click "Accept as Solution".