cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK V3 CN1 connector part number (male STDC14 pin )

Amrith
Associate II

I would like to know the connector CN1 the daughter board for stlink v3

I am attaching an image for reference. Kinldy anyone share the part number

2 REPLIES 2
netsbats
Associate II

That should fit: Samtec 

FLE-114-01-G-DV-P-TR

https://www.samtec.com/products/fle

Could also check BOM from NUCLEO-144 boards using ST-LINK/V3, so H743ZI2,  H723ZG

Header 5x2, 1.27mm, Dual row, Straight, Surface mount, vertical male connector. 3.05mm lead. Mates with FFSD connector. Footprint compatible with FTSH-107-01-L-DV,-K,-A,-P,-ES (STDC14 MEDIUM)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..