2014-06-25 12:20 AM
Hi guys,
I have been using the ST-Link debugger with the KEIL IDE (v5.11a) to develop some code for the Inemo-M1 development board.I had some issues trying to use the debugger with this version of Keil and when I contacted their help desk one of their personnel told me that ''MDK-ARM v5.11a is compatible with V2.J20.S0 but not with V2.J21.S0. Now the firmware on my ST-Link has been updated previously to version V2.J21.S4. The guy at KEIL cannot confirm whether this version is compatible with v5.11a and hence I would like to regress my version of ST-Link firmware to V2.J20.S0... Is this by any means possible?regards2014-06-25 03:30 AM
Is this by any means possible?
Yes, you just run an older firmware ''upgrade'' app at the desired level.[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/Downgrade%20ST-LinkV2%20firmware%20revision&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=251]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FDowngrade%20ST-LinkV2%20firmware%20revision&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=2512014-06-26 08:23 AM
Hi Emmanuel,
It’s a known limitation detected on MDK-ARMv
5.11 using ST-LINK (firmware version V2J21) with all STM32 devices.I recommend not using this version for the moment till fix of this problem. If this version is required, you can downgrade the ST-LINK FW to V2J20 using ST-LinkUpgrade.exe available at MDK-ARM v5.11 install directory at [Keil install directory]\ARM\STLink .
I will keep you informed once the problem fixed.
Best Regards, NouhaHi guys,
I have been using the ST-Link debugger with the KEIL IDE (v5.11a) to develop some code for the Inemo-M1 development board. I had some issues trying to use the debugger with this version of Keil and when I contacted their help desk one of their personnel told me that ''MDK-ARM v5.11a is compatible with V2.J20.S0 but not with V2.J21.S0. Now the firmware on my ST-Link has been updated previously to version V2.J21.S4. The guy at KEIL cannot confirm whether this version is compatible with v5.11a and hence I would like to regress my version of ST-Link firmware to V2.J20.S0... Is this by any means possible? regards2014-06-26 10:15 AM
I use another solution for this issue as I described at:
http://www.keil.com/forum/58066/ I discovered that: replace the Keil 5.11 ST-LINKIII-KEIL_SWO.dll v2.0.6.0 with the Keil 5.10 ST-LINKIII-KEIL_SWO.dll v2.0.4.0.