cancel
Showing results for 
Search instead for 
Did you mean: 

spirit 1 , and stm32f103xx?

TARHAN SAMAH
Senior
Posted on November 07, 2017 at 09:24

Hello every body we are using stm32f103xx microcontrollers , we want to send our data by wireless using spirit1 module ,

- is it possible ?

-which library is suitable ?

-what about distance amd range of gigahertz modules ?

urgent help needed plz thanks 

Samah Tarhan 

Argebilisim 

14 REPLIES 14
Posted on November 14, 2017 at 14:44

thanks  to all of you ok now i see better , we need to make it in two steps first send the firmware to the sp1ml via st link2 then use the uart in application mode like wireless uart ,,, i was really lost , im beginner ,, didnt know that urgent had a haker meaning , just my request was really huamnly urgent )) ..the support team of st helped me to see clearer .. thanks

Andrew Neil
Evangelist III
Posted on November 14, 2017 at 17:03

doumandjisamah wrote:

Argebilisim 

Is that this '

Argebilisim': 

http://www.argebilisim.com/en/index.html

 
TARHAN SAMAH
Senior
Posted on November 15, 2017 at 15:19

ok now i got the firmware and download the binary to the sp1ml using st-link , looks it is downloaded , now i want to test the AT COMMAND mode using the hyperterminal , first let me tell you the hardware connections pins :

-SHDN  connected to 3,3v , always power up 

-mode0 to 0, it is command mode

-vdd 3,3v 

-gnd to gnd 

-rx of spirit to tx of hyperterminal 

-tx of spirit to rx of hyperterminal 

-reset to button 3,3v to 0volts

i use baudrate 9600 and CR after sending :

,  i opened hyperterminal after reset i got '?',   so i entererd to command mode '+++' no answer , i tried AT nthg comes from spirit,??? is there something i missed 

Posted on November 15, 2017 at 14:58

YES Ä°T Ä°S we are in Istanbul, 

TARHAN SAMAH
Senior
Posted on November 16, 2017 at 12:27

Ä° SOLVE it it was a wrong adapter from hyperterminal to ttl , before i used adm now i use usb dongle ch340g or arduino adapter . now i communicate perfectly with my spirit 1 ,thanks