SPI Multi-master NSS Setup
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 12:48 AM
Hello
Im trying to implement stm32 spi multi-master function on a stm32f765 according to the below presentation
I keep getting MODF error when transmitting as a master, that would indicate that the slave sets the masters NSS pin low. Even if I set the NSS pin permantently high, by hooking it to a 3,3v pin , I get the same error!
below is my setup:
--------MSP SETUP--------------------------------------
GPIO_InitStruct.Pin = SPI_CS_Pin;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT | GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(SPI_CS_GPIO_Port, &GPIO_InitStruct);
// SPI master com trigger GPIO pin configuration
GPIO_InitStruct.Pin = SPI_MASTER_TRIG_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP ;
HAL_GPIO_Init(SPI_MASTER_TRIG_Port, &GPIO_InitStruct);
--------MSP SETUP--------------------------------------
------------SPI Handle setup--------------------------
static void setupSPIbaseStruct(SPI_HandleTypeDef *pSpiHandle, uint32_t mode)
{
pSpiHandle->Instance = SPI2;
if (mode == SPI_MODE_MASTER) {
pSpiHandle->Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
}else{
pSpiHandle->Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
}
pSpiHandle->Init.Direction = SPI_DIRECTION_2LINES;
pSpiHandle->Init.CLKPhase = SPI_PHASE_2EDGE;
pSpiHandle->Init.CLKPolarity = SPI_POLARITY_HIGH;
pSpiHandle->Init.DataSize = SPI_DATASIZE_8BIT;
pSpiHandle->Init.FirstBit = SPI_FIRSTBIT_MSB;
pSpiHandle->Init.TIMode = SPI_TIMODE_DISABLE;
pSpiHandle->Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE;
pSpiHandle->Init.CRCPolynomial = 7;
pSpiHandle->Init.NSSPMode = SPI_NSS_PULSE_DISABLED;
pSpiHandle->Init.NSS = SPI_NSS_HARD_INPUT;
pSpiHandle->Init.Mode = mode ;
}
------------SPI Handle setup--------------------------
what Im I doing wrong?
- Labels:
-
SPI
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 1:41 AM
Read out and check/post content of SPI and relevant GPIO registers.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 2:31 AM
Thank you for reply
A read out of NSS pin inside of error callback says pin is high, contrary to what should have triggered the error in question(MODF) modf(1) bit is set in Spihandle.ErrorCode
CR1 : 1010000100110011 / 0xa133
CR2: 1011100000000 / 0x1700
SR : 10 / 0x2
ErrorCode: 1 / 0x1
GPIO port IDR = 1
I don´t know if there´s any other relevant information?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 9:55 AM
Which pin is used for NSS? How is that pin's MODER and AFR set in GPIO?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 11:22 PM
The setup is the one I pasted in the code, the SPI_CS_Pin refers to GPIO_PIN_9 and SPI_CS_GPIO_Port to port GPIOB
and alternate function in use is AF5 according to the table below
- GPIO_InitStruct.Pin = SPI_CS_Pin;
- GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
- GPIO_InitStruct.Mode = GPIO_MODE_INPUT | GPIO_MODE_IT_RISING;
- GPIO_InitStruct.Pull = GPIO_PULLUP;
- HAL_GPIO_Init(SPI_CS_GPIO_Port, &GPIO_InitStruct);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-07 11:33 PM
I don't use Cube/HAL and don't understand it.
Read out and check/post the relevant register's content.
You want the pin to be set to AF in GPIO_MODER, and to proper AF in GPIO_AFR. My guess is, that this:
> GPIO_InitStruct.Mode = GPIO_MODE_INPUT | GPIO_MODE_IT_RISING;
does not do that.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-08 12:01 AM
So i guess we are on different sides of it, I can´t fully interpret the content of those registers:
GPIOx->MODER = 0xaaa06aa0 / 10101010101000000110101010100000
AFR = 0x40020020 / 1000000000000100000010000100000
AFR[0] = 0xa666900 / 1010011001100110100100000000
AFR[1] = 0x55bbbb00 / 1010101101110111011101100000000
What am I looking for? Thank you for helping!
EDIT: I see now that because Im setting Mode to GPIO_MODE_INPUT, the step where Alternate function is set is skipped. The reason why I set it to GPIO_MODE_INPUT and not GPIO_MODE_AF_PP was that I got strange behavior with the pin getting set half way (~2,2V / floating behavior), which disappeared when I set it to input.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-08 12:36 AM
How did you read that out? Did you use the debugger's register view?
AFR[1] = 0x40020020
This is suspiciously address of GPIOA->AFR[0].
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-08 12:40 AM
I updated the answer just before your post
I simply had a break point inside the setup function after the pin config
If your referring to the SFR view, that view does not show the GPIO registers:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-08 1:37 AM
> What am I looking for?
We are talking about PB9, so you want to look in MODER at bits 18 and 19 (i.e. 9*2 and 9*2+1 - two bits per pin are used), they are 0b00 which means Input, and are supposed to be 0b10 for AF. Then we would be looking at bits 4 to 9 in AFR[1] (4 bits per pin, that is 32 bits for pins PB0..PB7 in AFR[0] and 32 bits for pins PB8..PB15 in AFR[1].
Having no pin set to AF corresponding to the SPI2_NSS means, that internally that node is set to 0 - which immediately after enabling SPI switches it to slave mode.
> The reason why I set it to GPIO_MODE_INPUT and not GPIO_MODE_AF_PP was that I got strange behavior with the pin getting set half way (~2,2V / floating behavior), which disappeared when I set it to input.
I don't understand. If the PB9 is set as AF in MODER and AF5 in AFR[1], and SPI module is set so that NSS is input (i.e. SPI_CR2.SSOE=0), the PB9 pin works in exactly the same way as when it's set to Input. If not, some of those 3 things are not set in that way.
Do you have a pullup on that pin?
JW