2015-11-17 2:41 AM
Hey,
i have a stm32f407 board .Can anyone tell me whats the best way or possible ways to test the i2c and spi driver.2015-11-17 5:54 AM
Hi m.dums,
You can do some tests based on the examples that you may find in STM32CubeF4 package or F4 standard library.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-11-17 6:00 AM
what i mean is that, i dont have device that connected with spi or i2c interface. so i would like to know, is there any device that i can buy and test the driver ? or is there any solution other that connecting two boards ?
2015-11-17 6:10 AM
Isn't there a MEMS and CODEC devices you can talk too on the board? Use those.
Failing that get yourself some I2C or SPI FLASH/EEPROM devices and talk to those.