2010-08-23 11:09 AM
2011-05-17 05:04 AM
i have interfaced AT45DB161. i hv attached the code files (Read/ Write/ Device ID read functions) that might be helpful. change the PIN No.s
pullups are a not a problem.
tell me if u need more help.
2012-10-15 04:05 AM
Were you able to run on SPI1 PB3 - PB5?
2012-10-15 06:46 AM
Were you able to run on SPI1 PB3 - PB5?
On what part? On the F1 for instance you have to move the JTAG/SWD function off the pins. This is a very old thread, with a lot of content lost across several forum crashes so don't expect any of the original posters to respond. This thread deals with the JTAG remapping/disablinghttps://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F107VG PB3 - PB4 - PA15 Alternate Function Usage&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=278