2017-02-07 05:29 AM
In STM32F76xxx and STM32F77xxx silicon limitations DocID028806 Rev 4, 2.2.2 BSY bit may stay high at the end of a data transfer in slave mode which is entirely an SPI error, is listed under I2C peripheral limitations.
JW
Solved! Go to Solution.
2017-02-07 07:16 AM
Hi Jan,
Thanks for keeping this error to our attention: I confirm that the limitation 'BSY bit may stay high at the end of a data transfer in slave mode' is misplaced and should belong to SPI limitations.
This is noted and will be fixed in next errata version.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-02-07 07:16 AM
Hi Jan,
Thanks for keeping this error to our attention: I confirm that the limitation 'BSY bit may stay high at the end of a data transfer in slave mode' is misplaced and should belong to SPI limitations.
This is noted and will be fixed in next errata version.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.