source for TIMx UEV
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-10-28 2:49 PM
STM32F407xx
What are the sources for a TIMx update event?My specific use case is that I am using TIM3 to generate a quadrature encoder output (CC1 and CC2). See the earlier discussion on how to do this: (quadrature output - STM32F407). I am using an internal trigger to clock TIM1. TIM1 is set up to output a PWM signal based upon its input clock (TIM3). When I set CC1 as the trigger source, the output frequency from TIM1 is what I expect, but when I use the Update Event, it is doubled. This leads me to believe that I am either doing it wrong, and/or more than just the CNT=ARR generates an UEV.Any thoughts? #timer #stm32f4 #uev- Labels:
-
STM32F4 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-10-28 4:13 PM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/quadrature%20output%20-%20STM32F407&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=115]quadrature output - STM32F407 - cite
Well the toggle mode runs at 2x the frequency, is that what you mean? That's what allows the relative phase shift.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-10-29 1:31 AM
It's a rising edge of the trigger which advances the slave timer. If the master's CC mode is toggle, it generates a rising edge only once per two periods of the master timer; whereas the update is a *pulse* one timer cycle long, generated at each overflow of the timer, it means a rising edge at every period of the master timer.
JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-10-30 7:25 PM
Thanks Jan,
Your answer makes sense based upon what I was seeing. Have you seen documentation that says this?