2019-09-23 1:56 PM
Hello,
I am using NUCLEO-F429ZI. Can I use software to power off controller?
Regards,
2019-09-23 2:00 PM
You can put the chip in STANDBY
2019-09-24 10:35 AM
Hello, Clive:
thank you for your response.
I try to add the following code to enter standby mode
//disable wake-up timer
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
//diable RTC Alarm
HAL_RTC_DeactivateAlarm(&hrtc,RTC_FLAG_ALRAF);
//clear PWR FLAG
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
//enable WKUP pin
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
//enter standby mode
HAL_PWR_EnterSTANDBYMode();
//
//turn off led 2
GPIOB->BSRR = (uint32_t)LD2_Pin << 16U;
but I still have 1mA current when I put battery in my system. Do you have any idea to reduce current when only battery is connected to controller?
thank you in advance.
2019-09-25 4:32 AM
DBGMCU->CR = 0; // Disable debug and trace in low-power modes
Do this before entering low-power mode.