cancel
Showing results for 
Search instead for 
Did you mean: 

SMT32F407VGT6 / CAN issue

JACK00
Associate II

主控板 (SMT32F407VGT6)与同服板 (STM32F407VGT6) 之间的CAN通讯,环境温度低于-10度,通讯不正常,环境温度高过-10度!

4 REPLIES 4
SofLit
ST Employee

Hello @JACK00 ,

In next time, could you please describe your issue in English as other community members can help you?

Translation:

"The CAN communication between the main control board (SMT32F407VGT6) and the server board (STM32F407VGT6), the ambient temperature is lower than -10 degrees, the communication is abnormal, and the ambient temperature is higher than -10 degrees!"

Not sure the question is clear. Could you please elaborate more?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!

Dupe  https://community.st.com/t5/stm32-mcus-products/smt32f407vgt6/td-p/624102

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

What is your clock source? HSI or HSE?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.