2024-01-01 11:09 PM - last edited on 2024-01-02 2:02 AM by mƎALLEm
The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!
2024-01-01 11:41 PM
Check performance of external clock and transceiver.
You can output HSE via PA8 (MCO) and check clock accuracy within specification limits.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.