2023-10-03 11:52 PM
<Question>
Could not find SMBus parameter setting MENU when I2C as a SMBus 2-wire mode.
Solved! Go to Solution.
2023-10-09 2:01 AM
Hello All,
Thank you @kim1 for bringing this issue to our attention with detailed explanation.
Issue is reproduced and escalated to Development team in internal ticket ID163042 for fix.
(PS: ID163042 is an internal tracking number and is not accessible or usable by customers).
Thanks
Imen
2023-10-04 12:33 AM
Welcome @kim1, to the community!
Which version of STM32CubeMX or STM32CubeIDE are you using?
The parameters of the SMBus slave features should expand when you click the little triangle (or arrow) to the left of the line. You can also set only the primary slave address there.
Regards
/Peter
2023-10-04 3:19 AM
2023-10-04 7:57 AM
This is indeed interesting and should to be checked.
2023-10-06 1:27 AM
Please update if there is anything helpful.
Thank you and Regards
2023-10-09 2:01 AM
Hello All,
Thank you @kim1 for bringing this issue to our attention with detailed explanation.
Issue is reproduced and escalated to Development team in internal ticket ID163042 for fix.
(PS: ID163042 is an internal tracking number and is not accessible or usable by customers).
Thanks
Imen
2023-10-10 6:05 PM
Thank you team!!