cancel
Showing results for 
Search instead for 
Did you mean: 

Simple Multicore Core to Core Communication with STM32H7

JR1
Associate II

Hello Team,

 

how can a simple core to core communication on the STM32H7 be implemented? We want to exchange 2kByte of data in bidirectional way between CM7 and CM4.

Best regards,

Jochen

12 REPLIES 12
JR1
Associate II

Where do I find the places in the code for the data array (memory) which is exchanged?

Is the same data array used for both exchanged data between the 2 cores?

JR1
Associate II

Is there any simpler solution available for the shared mermory access? We just want to exchange 2KByte of data between the 2 cores.

See this thread: https://community.st.com/t5/stm32cubeide-mcus/easiest-way-to-share-data-between-cores-in-stm32h745/td-p/576140

Or just create a shared memory region common to the two cores on each Core's linker. But you need to ensure at least two things:

- Synchronization of read and write operation between the two cores using HSEM to ensure the consistency of the data.

- Either to manage the data coherency from CM7 side when Cache is enabled or declare that region as Strongly-Ordered or Device (non cacheable) using MPU.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.