2024-09-06 12:41 AM
Hello Team,
how can a simple core to core communication on the STM32H7 be implemented? We want to exchange 2kByte of data in bidirectional way between CM7 and CM4.
Best regards,
Jochen
Solved! Go to Solution.
2024-09-08 9:58 PM
Where do I find the places in the code for the data array (memory) which is exchanged?
Is the same data array used for both exchanged data between the 2 cores?
2024-09-09 1:53 AM
Is there any simpler solution available for the shared mermory access? We just want to exchange 2KByte of data between the 2 cores.
2024-09-09 2:16 AM
Or just create a shared memory region common to the two cores on each Core's linker. But you need to ensure at least two things:
- Synchronization of read and write operation between the two cores using HSEM to ensure the consistency of the data.
- Either to manage the data coherency from CM7 side when Cache is enabled or declare that region as Strongly-Ordered or Device (non cacheable) using MPU.