cancel
Showing results for 
Search instead for 
Did you mean: 

Setting the F407 FSMC WaitSignalPolarity default value

Toneski
Associate II

Hi All,

I have a 407 connected to an FPGA using the FSMC interface.

When I compile my device configuration from ST Cube, the WaitSignalPolarity value in the MX_FSMC_Init routine is always set to: FSMC_WAIT_SIGNAL_POLARITY_LOW. On my system I need this setting to be FSMC_WAIT_SIGNAL_POLARITY_HIGH, but cannot find a way of setting this value through CubeMX.

Has anyone else found this issue or know how to fix it? Its getting a real pain having to manually update the source code before recompiling.

Kind Regards,

Tony

12 REPLIES 12
FBL
ST Employee

Hello @Toneski 

 

Could you please share a screenshot of the FMC peripheral registers?

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Toneski
Associate II

Hi,

How do you mean a screen shot? As a capture from within a debug session or a configuration settings view.

In case you need how the FSMC is setup, I attach the code that I use for configuration:-

hsram1.Init.NSBank = FSMC_NORSRAM_BANK1;

hsram1.Init.DataAddressMux = FSMC_DATA_ADDRESS_MUX_ENABLE;

hsram1.Init.MemoryType = FSMC_MEMORY_TYPE_PSRAM;

hsram1.Init.MemoryDataWidth = FSMC_NORSRAM_MEM_BUS_WIDTH_16;

hsram1.Init.BurstAccessMode = FSMC_BURST_ACCESS_MODE_ENABLE;

hsram1.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_HIGH;

hsram1.Init.WrapMode = FSMC_WRAP_MODE_DISABLE;

hsram1.Init.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS;

hsram1.Init.WriteOperation = FSMC_WRITE_OPERATION_ENABLE;

hsram1.Init.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE;

hsram1.Init.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE;

hsram1.Init.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_DISABLE;

hsram1.Init.WriteBurst = FSMC_WRITE_BURST_ENABLE;

hsram1.Init.PageSize = FSMC_PAGE_SIZE_NONE;

 

This is how I need the FSMC setup. After re-compiling the code from the IDE, I get exactly the same, but with:-

hsram1.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_LOW;

Set.

 

Applogies for the delay in replying - I've only just noticed.

Regards,

 

 

 

FBL
ST Employee

Yess @Toneski . This would be helpful to follow up on this case.

FBelaid_0-1701173319057.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Toneski
Associate II

Hi F.Belaid,

Please find attached a register dump of the FSMC as setup for my project.

Hope this helps.

Regards, Toneski.

Toneski
Associate II

...Another copy, but with BCR1 expanded.

Toneski_0-1701180959727.png

 

FBL
ST Employee

Hello @Toneski 

 

Could you check that the memory being used, actually, our controller does not support cross boundary page for Cellular RAM 1.5.

Also, using multiplexed IOs PSRAM, could you please check the address bus A[25,16].

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Toneski
Associate II

Hi @FBL,

I am not using memory through the FSMC (well - none that is directly usable as memory for the CPU) - as per the initial post, I am accessing an FPGA through the FSMC. 

Everything I need can be accessed through a 64K page, so I haven't investigated A[25:16] - as long as the FSMC triggers the external chip select when accessing 0x6000xxxx I'm happy.

Everything works fine, except that the WaitSignalPolarity value in the MX_FSMC_Init routine is always set to: FSMC_WAIT_SIGNAL_POLARITY_LOW. 

Would it be possible to have this setting to be FSMC_WAIT_SIGNAL_POLARITY_HIGH - I cannot find a way of setting this value through CubeMX.

Does this help at all?

Regards,

Toneski

FBL
ST Employee

Hello again @Toneski 

Could you please share your IOC file? For instance, you can force it in user defined code. It should not get changed after regenerating the code.

 

  /* USER CODE BEGIN FSMC_Init 2 */
  hsram1.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_HIGH;

    if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)
  {
    Error_Handler( );
  }
  /* USER CODE END FSMC_Init 2 */

 

Which CubeIDE version do you use?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Toneski
Associate II

Hi @FBL,

I thought about setting it within a USER CODE segment, but there isn't one between the value getting set and the call to HAL_SRAM_Init as shown here...

 

hsram1.Init.BurstAccessMode = FSMC_BURST_ACCESS_MODE_ENABLE;

hsram1.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_HIGH;

hsram1.Init.WrapMode = FSMC_WRAP_MODE_DISABLE;

hsram1.Init.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS;

hsram1.Init.WriteOperation = FSMC_WRITE_OPERATION_ENABLE;

hsram1.Init.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE;

hsram1.Init.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE;

hsram1.Init.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_DISABLE;

hsram1.Init.WriteBurst = FSMC_WRITE_BURST_ENABLE;

hsram1.Init.PageSize = FSMC_PAGE_SIZE_NONE;

/* Timing */

Timing.AddressSetupTime = 15;

Timing.AddressHoldTime = 15;

Timing.DataSetupTime = 255;

Timing.BusTurnAroundDuration = 0;

Timing.CLKDivision = 4;

Timing.DataLatency = 2;

Timing.AccessMode = FSMC_ACCESS_MODE_A;

/* ExtTiming */

 

if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)

{

Error_Handler( );

}

/* USER CODE BEGIN FSMC_Init 2 */

 

I am using CubeIDE Version: 1.13.1 - Build: 17479_20230728_0839 (UTC)

I've attached my IOC file...

Regards,

Toneski.