2016-01-05 08:35 PM
Hi Everyone,
Is there a way of using Terminal I/O feature of IAR(or any other)to send large input values(string or binary)) to function getting executed on STM32 Nucleo board.The input values being read from the text file placed on the Development PC.This is required to test some image processing functions in IAR which requires lot of Test data to be processed inside the code running on IAR.Thanks in advance !Rgds,Rp #nucleo #iar #keil #!stm32 #stm32cubemx