cancel
Showing results for 
Search instead for 
Did you mean: 

Secure boot for STM32H745

ATank.1
Associate III

Hello Team,

We are developing a bootloader for STM32H745 MCU. Follwoing are requirements,

 

1. SDcard will contain the images for M7, M4 and External QSPI flash connected to H745 MCU

2. Planning to use Secure boot such as SBSFU. Please suggest if this is fine or any other option for secure boot considering available reference codes etc.

3. Bootloader will have touchGFX for displaying firmware upgrade progress

 

Please suggest reference codes available which can be refered for SBSFU

Thanks & Regards, 

 Anuj

0 REPLIES 0