2024-10-03 11:56 PM
Hi,
uc: stm32f446
I have a question regarding non standard word length over RS485.
I need to receive next frame over RS485
1 start bit, 16-bit data word, 2 stop bits, in total 19 bits.
UART implementation allows to receive 8 or 9-bit data words.
Could you please advice what can be an approcach to achieve?
Best regards, Taras.
2024-10-11 5:43 PM
This chip is sp3845
2024-10-14 7:48 AM
@zhaowhong wrote:This chip is sp3845
That's just an RS485 transceiver; that has nothing to do with the data frame format - just the voltages used to represent the bit states.
2024-10-14 10:47 AM
You are quite right - in this particular case we have voltages and edge detection.
2024-10-14 11:12 AM
So, again, what was your basis for saying, "The real product does not do this"
What does the "real product" do?
2024-10-14 11:14 AM
I had a uart with non-standard word length( 16 bits ). This is all it does.
2024-10-14 11:23 AM
Sorry, it was @zhaowhong who said, "The real product does not do this"
But can't you give any more detail of what you do have than just, "Fanuc encoder"?
A part number? A link to a datasheet or Product Page? Anything??