cancel
Showing results for 
Search instead for 
Did you mean: 

RMII diagrams

StefanoRossi
Associate

Hi, we are working with a STM32F217 and the RMII bus.

In the two documents reported I see an inconsistency on the diagrams (on the one hand rising edge sampling, on the other falling edge). Which one is correct for my chip?

RM0033 Figure 328 Reference Manual (01 Mar 2021) 

DS6697 Figure 48Product Specification (05 Sep 2016) 

 

BR

Stefano

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hi @StefanoRossi ,

The RMII operates using the rising edge of the clock signal for both TX and RX data transfers.

So, the DS6697 Rev 13 - Figure 48. Ethernet RMII timing diagram is the correct one.

This RM0033 will be updated to fix the issue.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @StefanoRossi and welcome to ST Community,

Thank you for having reported the point.

I escalated this request to involved people for review and take the necessary action.

(Internal ticket number: 191487 - this ticket number is only for reference, not available outside of ST)

I'll make sure to post updates here as soon as possible. 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hi @StefanoRossi ,

The RMII operates using the rising edge of the clock signal for both TX and RX data transfers.

So, the DS6697 Rev 13 - Figure 48. Ethernet RMII timing diagram is the correct one.

This RM0033 will be updated to fix the issue.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen