2024-10-04 12:42 AM - last edited on 2024-10-04 2:08 AM by mƎALLEm
I am using stm32f103c8t6 microcontroller for uploading the bootloader and application. After uploading the bootloader binary code using UART communication (boot1=0 and boot0=1) to the controller, the reset pin is not working for further functionality i.e it is not erasing the current program and the uploaded code is working after pressing the reset button. Please guide me regarding that problem.
Solved! Go to Solution.
2024-10-04 3:38 AM
Ok,
I had a doubt you are using Blue pill board: https://stm32-base.org/boards/STM32F103C8T6-Blue-Pill.html
and you confirmed it.
At this stage, I can only suggest you (as I mentioned previously) to check reset pin level according to the user button state. If it doesn't present issue, so I suspect you are facing a fake MCU. So I recommend you to purchase a genuine product such as NUCLEO-F103RB board.
See for example this thread.
2024-10-04 12:51 AM
Hello @Shaktimayee and welcome to the community,
What do you mean by "reset erasing program":
@Shaktimayee wrote:
the reset pin is not working for further functionality i.e it is not erasing the current program and the uploaded code is working.
2024-10-04 12:57 AM
Sounds normal, and reset shouldn't erase the part.
Are you driving the RESET pin? How and to what is it connected?
The BOOTx pins will determine what is run out of reset.
2024-10-04 1:24 AM
thank you for your reply!!!! have you any idea regarding the original bootloader code for the stm32f103c8t6 microcontroller for the system memory!!?
2024-10-04 1:25 AM
yes i am driving the RESET button as the reset pin.
2024-10-04 1:47 AM
Hello,
Sorry still not able to understand your question.
I propose to refer to these application notes:
2024-10-04 1:55 AM
Only a button to ground, with a pull-up, or connected to anything else in your circuit?
2024-10-04 2:05 AM
I am uploading the code present in this link:- "https://www.youtube.com/watch?v=ppQx_scTsvQ"
for the bootloader and the application. For another operation let if i want to use my stm32f103c8t6 board for another program or if i am resetting the controller by pressing the RESET pin it is not working for which i am unable to upload the programme using the UART communication. Please guide me regarding that.
2024-10-04 2:08 AM
After using the code present in the link " https://www.youtube.com/watch?v=ppQx_scTsvQ"
controller's RESET pin is not working for another program to upload the code or flash the code in the controller using UART.
2024-10-04 2:28 AM
Did you set back boot0=0 ?