cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX Error with RVT70HSSNWC00-B and STM32H757XIH6

paweljaromin
Visitor

Hello,

I’m using the RVT70HSSNWC00-B from Riverdi and STM32H757XIH6 (datasheet: https://download.riverdi.com/RVT70HSSNWC00-B/DS_RVT70HSSNWC00-B_Rev.1.3.pdf ). After generating the project, regardless of the TouchGFX version (4.24.2, 4.24.0), I encounter the following error:

        CM7/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc\libtouchgfx-float-abi-hard.a(LCD24bpp.o): In function `touchgfx::LCD24bpp::DecompressorRGB_QOI::blitCopyARGB8888(unsigned char const*, touchgfx::Rect const&, touchgfx::Rect const&, unsigned char)':

  (.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI16blitCopyARGB8888EPKhRKNS_4RectES6_h+0x328): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'

        (.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI16blitCopyARGB8888EPKhRKNS_4RectES6_h+0x4e2): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'

        CM7/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc\libtouchgfx-float-abi-hard.a(LCD24bpp.o): In function `touchgfx::LCD24bpp::DecompressorRGB_QOI::blitCopyRGB888(unsigned char const*, touchgfx::Rect const&, touchgfx::Rect const&, unsigned char)':

        (.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI14blitCopyRGB888EPKhRKNS_4RectES6_h+0x46a): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'

        (.text._ZN8touchgfx8LCD24bpp19DecompressorRGB_QOI14blitCopyRGB888EPKhRKNS_4RectES6_h+0x4ea): undefined reference to `touchgfx::paint::flushLine(unsigned long*, int)'

 

Depending on the TouchGFX version, I use the corresponding STM32CubeMX version. After generating the code, the project can be uploaded to the controller, but the touch functionality does not work. I’ve already tried various combinations, including migrating projects to newer versions. Unfortunately, nothing seems to work.

 

Does anyone have any idea what might be wrong? Any help would be greatly appreciated.

Thank you in advance!

Let me know if you'd like any adjustments.

 

Pawel Jaromin

0 REPLIES 0