cancel
Showing results for 
Search instead for 
Did you mean: 

Request for enhancement : Cube 4.21.0

Posted on May 30, 2017 at 19:11

Eric,

In the implementation that was included in 4.21 there was a couple of MISRA violations inserted.

Unlike the assert_failed routine, _Error_Handler uses char* and int for parameters instead of uint8_t* and uint32_t.

Just a head-up.

Also, the USER CODE BEGIN and USER CODE END comments have an incorrect function name.

Andrei

1 REPLY 1
Imen.D
ST Employee
Posted on May 30, 2017 at 22:49

Hi

Chichak.Andrei

,

Thank you for your reported issue.

I will forward your request internally to our CubeMx team.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen