2018-08-21 2:56 AM
Hi
I have recollections from a while ago, that it is possible to have an ST Link connected to one PC, and connect to it via ST Link server from another PC via a network. I have spent alot of time searching trying to find some information on this but have not been successful.
So my question is: Is it possible to have an ST Link connected to a usb port on a linux (ubuntu) system, and connect to that ST link via a network connection from a Windows (7) system? The IDE I am using is Atollic Studio. Can someone recoomand where I can find or provide some instructions on how to do this please?
Thanks in advance
Andrew
2018-08-21 4:01 AM
If I recall correctly, Atollic uses gdb. If this is true, you can run a gdb server on linux (e.g. openocd) and attach to that from Atollic. That answers the "is is possible part"; the specific details you'll have to work out.
2018-08-21 8:43 AM
Hi Geoffrey
Thank you for your reply. Your suggestion of "openOCD" was they key and after a search I have found this page which has helped a bit https://gnu-mcu-eclipse.github.io/openocd/install/
Currently I get this error when I try and connect:
"Failed to execute MI command:
target extended-remote localhost:3333
Error message from debugger back end:
localhost:3333: The system tried to join a drive to a directory on a joined drive."
I've not found a solution yet which fixes the problem. When I do I'll post it here
2018-08-21 9:37 AM
The ST-LINK firmware can be updated to J-Link OB, that might provide additional options/paths
2024-04-12 11:35 AM - edited 2024-04-12 11:42 AM
Something about this thread bothers me. Since stlink-server does its ide/daemon comms via TCP we SHOULD be able to run the ide on any other network connected PC and have the target board and stlink-server running from a separate PC, only using the stlink-server deamon as the gateway.
Unfortunately the stlink-server options only support [-p tcpport] and defaults to the loopback address 127.0.0.1. This makes it impossible to do remote PC debugging without resorting to iptables port forward trickery.
It seems very shortsighted that the stlink-server daemon doesn't allow selection of the listenning address as well as the port.
My point is that openOCD running on the target host PC should not be necessary if stlink-server simply provided the ability to bind a generic IP address.
2024-04-12 12:52 PM
I mean you miss. I use it on windows and in config.txt set port only. But it works ok for all interfaces.
@Echo off
cmd /K "ST-LINK_gdbserver.exe -c config.txt || echo GDB server exited"
2024-04-12 2:14 PM
@MM..1I have no idea what you are saying.
1) is stlink-server a USB/TCP bridge application or is it a full-fledged GDBserver and USB/TCP bridge? If if is a gdbserver then its utility is limited by not allowing binding to a routable IP address.
2) If the remote host (the one running stlink-server and having the target board connected via USB) must have an intermediary gdbserver instance running on it to bridge stlink-server and the (IDE running on a different PC) then there needs to be documentation on what that gdbserver setup is...It still should not require openOCD.
2024-04-12 11:19 PM - edited 2024-04-12 11:34 PM
2024-04-13 8:48 AM
re - DM00613038 ... Thanks. Will take a look.