2021-04-10 05:11 AM
Hello,
i would like to know why after st-link programer has been cut-off usart1(pa9,pa10) and usart3(pb10,pb11) doesn't work at all.
Any help would be appreciated.
Thanks
2021-04-10 06:31 AM
IO side power supply
Double check the schematic, and probe salient points on the PCB
2021-04-10 06:55 AM
Thanks for the prompt reply.
For now, i don't have any probe to test with.
The board is powered with 5V on E5V and i've also done some tests with 3V but none of them work.
I don't know where or what to look for.
2021-04-10 08:15 AM
Perhaps you can expand on the testing you did to determine how USART1 and USART3 failed, how you have them wired up and to what.