2010-07-28 02:30 PM
Raisonance Ride 7 and Rkit ARM - what are the limitations ?
2011-05-17 05:00 AM
hello,
you have a code limitation of 32kb for free version, one license is about 700€. regards2011-05-17 05:00 AM
code limitation of 32kb is only for debugging, while there is no limit for compilation. you can compile bigger codes but cannot debug code bigger than 32KB in free license.
regards2011-05-17 05:00 AM
As far as I can see from the license, the code limitation of 32KB applies whether or not you want debugging or not. I disabled the generation of debug information and still ran into the 32KB limitation when linking in uVersion. So, be careful of the limitations here.
2011-05-17 05:00 AM
hello
do I have to buy JTAG adapter for debug ? and which model do I have to buy for STM32 ? how much is it ?2011-05-17 05:00 AM
''ran into the 32KB limitation when linking in uVersion (sic)''
I take it you mean, uVision? But uVision is a Keil product - it has absolutely nothing whatsoever to do with the Raisonance products that the OP is asking about!! Licence restrictions are entirely a matter for the specific product providers - so you really need to talk direct to them for questions like this!