cancel
Showing results for 
Search instead for 
Did you mean: 

Raisonance Ride 7 and Rkit ARM - what are the limitations ?

mehmet.karakaya
Associate III
Posted on July 28, 2010 at 23:30

Raisonance Ride 7 and Rkit ARM - what are the limitations ?

5 REPLIES 5
rodolphe
Associate II
Posted on May 17, 2011 at 14:00

hello,

you have a code limitation of 32kb for free version, one license is about 700€.

regards

kashif
Associate II
Posted on May 17, 2011 at 14:00

code limitation of 32kb is only for debugging, while there is no limit for compilation. you can compile bigger codes but cannot debug code bigger than 32KB in free license.

regards

jingzhao
Associate
Posted on May 17, 2011 at 14:00

As far as I can see from the license, the code limitation of 32KB applies whether or not you want debugging or not. I disabled the generation of debug information and still ran into the 32KB limitation when linking in uVersion. So, be careful of the limitations here. 

mehmet.karakaya
Associate III
Posted on May 17, 2011 at 14:00

hello

do I have to buy JTAG adapter for debug ?

and which model do I have to buy for STM32 ?

how much is it ?

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:00

''ran into the 32KB limitation when linking in uVersion (sic)''

 

I take it you mean, uVision?

But uVision is a Keil product - it has absolutely nothing whatsoever to do with the Raisonance products that the OP is asking about!!

Licence restrictions are entirely a matter for the specific product providers - so you really need to talk direct to them for questions like this!