2024-07-15 08:23 AM
Hello,
I am facing constant difficulties in connecting to my Nucleo H723ZG Boards.
Almost every time I try to update the ST-Link via STMCube32IDE, the compilation stops half-way through the process and throws an error (see image)
I have tried:
It appears to be, that a successfull connection happens almost randomly and about 1 out of 10 tries.
Has anyone faced the same issue?
Thanks
2024-07-15 08:42 AM
Seems to be already at the same level.
Do with the upgrade app directly, without any secondary connectivity or daemon trying to connect.