2024-01-27 4:43 AM
Hello,
I try to trace the GPIO pin status in Keil5 MDK ARM logic analyzer, but it's not successful.
I am using the Nucleo-H743ZI2 board with STLink 3 SWO mode. I can also see the printf output in the "Debug (printf) Viewer" without any issue. The LED on board is on PB0. In the debug mode, I can see the GPIOB ODR is updating, which aligns with the LED status.
But when I type the "PORTB.0" in the Logic Analyzer setup, it said "Unknown signal".
Is there a way to trace the GPIO pin status in the logic analyzer by Keil5 MDK ARM? I tried "PORTB.0", "GPIOB.0", etc, but none of them works.
Thanks in advance.
BR,
JN
2024-01-27 5:12 AM
Note that Keil Tools are from an independent company - nothing to do with ST.
For questions about the Keil tools, try:
https://community.arm.com/support-forums/f/keil-forum