2024-09-05 4:23 AM
i'm using Stm-Cube ide version 1.15.0 and getting this error when trying to flash the firmware.
2024-09-05 5:40 AM
Can you connect using the standalone STM32CubeProgrammer program?
What does test.elf do? If it goes into low power modes, or re-initialized SWD pins, or erases FLASH, this will cause issues with debug.
Is this a known good ST board or custom hardware?
2024-09-06 1:44 AM
it is a nucleo board-L452RET6
2024-09-06 5:43 AM
And the answers to the other questions?
2024-09-21 8:29 AM
sorry for the late reply.
https://community.st.com/t5/stm32-mcus-products/quot-failed-to-execute-mi-command-load-failed-ltdc-paint-elf/td-p/94809
this helped me to clear the error
Thanks for the reply