cancel
Showing results for 
Search instead for 
Did you mean: 

"Failed to execute MI command ...error from the debuggers end"

Harumoto_2
Visitor

i'm using Stm-Cube ide version 1.15.0 and getting this error when trying to flash the firmware.

Harumoto_2_0-1725535213578.png

 

1 REPLY 1
TDK
Guru

Can you connect using the standalone STM32CubeProgrammer program?

What does test.elf do? If it goes into low power modes, or re-initialized SWD pins, or erases FLASH, this will cause issues with debug.

Is this a known good ST board or custom hardware?

If you feel a post has answered your question, please click "Accept as Solution".