2022-04-12 11:18 PM
Hi,
I am trying to connect to a 16 bit parallel display interface. To write new data, I have to use pins on five different ports (GPIOs A, B, C, D, E). Right now I am setting these pins like this:
PORT_D15->BSRR = (PIN_D15 << 16) | (((data >> 15) & 0x01) * PIN_D15) ;repeat for all other 15 pins.
This is causing the display to update slowly, you can see the screen 'rolling in' from the top.
On a previous controller all pins were in one port, and one access to
PORT_DISPLAY->ODRwas enough to set all pins.
Is there a quicker way to set all those port pins?
Solved! Go to Solution.
2022-04-19 2:35 AM
mask is a constant, so no need to AND it.
But yes, you are right, data would need to be masked with the same mask. Okay, so that's one more AND.
Still, the negation, masking AND and left-shift for the BRx portion would be spared down.
JW
2022-04-19 2:35 AM
Thanks, Jan. That indeed was a "typo" - initial version was a bit different, I edited it and left the wrong operator. Fixed it now.
By the way, the code will work even if mask is not a constant, but of course there will be an additional shift operation done at runtime.
2022-04-19 2:42 AM
If the data variable can have non-display bits set, then indeed you have to do it, but that's and additional operation. As you are asking for quickest way, it's better to ensure the data variable only uses the display related bits.
Actually the absolute quickest way is the one suggested by user ".". Lock the non-display pins at the port and just write data to ODR register. Sorry, this is also wrong because locking lock only the configuration registers, not data registers. Reference manual:
The frozen registers are GPIOx_MODER, GPIOx_OTYPER, GPIOx_OSPEEDR, GPIOx_PUPDR, GPIOx_AFRL and GPIOx_AFRH.
2022-04-19 5:48 AM
I just tried to implement it and I think this approach overlooks the fact, that my pins are not in order.
So lets say, the used display pins on GPIOC are on PC2, PC7, PC12, however PC2 has Bit4, PC7 has Bit12 and PC12 has Bit9 of the parallel data to be written.
masking GPIOC->BSRR works for the higher reset pins, but when it comes to setting, I can't see a way to mask the data, so that the pins are set correctly right away.
To me it seems there still has to be the assignment of pins like in TDKs answer.
So this would only work if PC2 was databit2, PC7 data bit 7 and PC12 bit 12.
2022-04-19 6:04 AM
Store data in memory with bits in the order of display.
Or...
...you can increase your pain...
JW
2022-04-19 6:15 AM
unfortunately also not possible since PC12 has bit9 and PB12 has bit 15.
only way would be to have separate data arrays for every port and that would require getting those from the original data variable, which would be just as costly as the usual bit shifts.
It seems increasing my pain is the only outcome here
2022-04-19 6:19 AM
Post the exact layout and your current solution together with disasm (mixed with source would be the best), with some benchmark.
JW
2022-04-19 7:16 AM
So the subjectively quickest way looks like this:
pin defines
#define ILI9341_PORT_D0 GPIOB
#define ILI9341_PORT_D1 GPIOE
#define ILI9341_PORT_D2 GPIOE
#define ILI9341_PORT_D3 GPIOB
#define ILI9341_PORT_D4 GPIOC
#define ILI9341_PORT_D5 GPIOA
#define ILI9341_PORT_D6 GPIOB
#define ILI9341_PORT_D7 GPIOD
#define ILI9341_PORT_D8 GPIOD
#define ILI9341_PORT_D9 GPIOC
#define ILI9341_PORT_D10 GPIOC //changed, orig GPIOA
#define ILI9341_PORT_D11 GPIOA
#define ILI9341_PORT_D12 GPIOC
#define ILI9341_PORT_D13 GPIOB
#define ILI9341_PORT_D14 GPIOB
#define ILI9341_PORT_D15 GPIOB
#define ILI9341_PIN_D0 GPIO_PIN_11
#define ILI9341_PIN_D1 GPIO_PIN_11
#define ILI9341_PIN_D2 GPIO_PIN_9
#define ILI9341_PIN_D3 GPIO_PIN_2
#define ILI9341_PIN_D4 GPIO_PIN_2
#define ILI9341_PIN_D5 GPIO_PIN_0
#define ILI9341_PIN_D6 GPIO_PIN_4
#define ILI9341_PIN_D7 GPIO_PIN_7
#define ILI9341_PIN_D8 GPIO_PIN_4
#define ILI9341_PIN_D9 GPIO_PIN_12
#define ILI9341_PIN_D10 GPIO_PIN_11
#define ILI9341_PIN_D11 GPIO_PIN_8
#define ILI9341_PIN_D12 GPIO_PIN_7
#define ILI9341_PIN_D13 GPIO_PIN_13
#define ILI9341_PIN_D14 GPIO_PIN_14
#define ILI9341_PIN_D15 GPIO_PIN_12static uint8_t ili9341_Write(uint16_t data) {
GPIOA->BSRR = (ILI9341_PIN_D5 << 16) >> (((data >> 5) & 0x01) * 16) |
(ILI9341_PIN_D11 << 16) >> (((data >> 11) & 0x01) * 16);
GPIOB->BSRR = (ILI9341_PIN_D3 << 16) >> (((data >> 3) & 0x01) * 16) |
(ILI9341_PIN_D0 << 16) >> (((data >> 0) & 0x01) * 16) |
(ILI9341_PIN_D6 << 16) >> (((data >> 6) & 0x01) * 16) |
(ILI9341_PIN_D13 << 16) >> (((data >> 13) & 0x01) * 16) |
(ILI9341_PIN_D14 << 16) >> (((data >> 14) & 0x01) * 16) |
(ILI9341_PIN_D15 << 16) >> (((data >> 15) & 0x01) * 16);
GPIOC->BSRR = (ILI9341_PIN_D4 << 16) >> (((data >> 4) & 0x01) * 16) |
(ILI9341_PIN_D9 << 16) >> (((data >> 9) & 0x01) * 16) |
(ILI9341_PIN_D10 << 16) >> (((data >> 10) & 0x01) * 16) |
(ILI9341_PIN_D12 << 16) >> (((data >> 12) & 0x01) * 16);
GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
(ILI9341_PIN_D7 << 16) >> (((data >> 7) & 0x01) * 16);
GPIOE->BSRR = (ILI9341_PIN_D1 << 16) >> (((data >> 1) & 0x01) * 16) |
(ILI9341_PIN_D2 << 16) >> (((data >> 2) & 0x01) * 16);
ILI9341_PORT_WR->BSRR = (ILI9341_PIN_WR << 16)
| (ILI9341_WR_LOW * ILI9341_PIN_WR);
ILI9341_PORT_WR->BSRR = (ILI9341_PIN_WR << 16)
| (ILI9341_WR_HIGH * ILI9341_PIN_WR);
return 1;
}disassembly in next post
2022-04-19 7:17 AM
08005512: mov.w r7, #268435456 ; 0x10000000
125 GPIOB->BSRR = (ILI9341_PIN_D3 << 16) >> (((data >> 3) & 0x01) * 16) |
08005516: ubfx r1, r0, #3, #1
126 (ILI9341_PIN_D0 << 16) >> (((data >> 0) & 0x01) * 16) |
0800551a: lsls r3, r3, #4
130 (ILI9341_PIN_D15 << 16) >> (((data >> 15) & 0x01) * 16);
0800551c: lsls r4, r4, #4
0800551e: asr.w r4, r7, r4
125 GPIOB->BSRR = (ILI9341_PIN_D3 << 16) >> (((data >> 3) & 0x01) * 16) |
08005522: mov.w lr, #262144 ; 0x40000
126 (ILI9341_PIN_D0 << 16) >> (((data >> 0) & 0x01) * 16) |
08005526: asr.w r3, r12, r3
133 (ILI9341_PIN_D9 << 16) >> (((data >> 9) & 0x01) * 16) |
0800552a: ubfx r2, r0, #9, #1
125 GPIOB->BSRR = (ILI9341_PIN_D3 << 16) >> (((data >> 3) & 0x01) * 16) |
0800552e: lsls r1, r1, #4
08005530: asr.w r1, lr, r1
129 (ILI9341_PIN_D14 << 16) >> (((data >> 14) & 0x01) * 16) |
08005534: orrs r3, r4
133 (ILI9341_PIN_D9 << 16) >> (((data >> 9) & 0x01) * 16) |
08005536: lsls r2, r2, #4
08005538: asr.w r5, r7, r2
0800553c: orrs r3, r1
132 GPIOC->BSRR = (ILI9341_PIN_D4 << 16) >> (((data >> 4) & 0x01) * 16) |
0800553e: and.w r2, r0, #16
134 (ILI9341_PIN_D10 << 16) >> (((data >> 10) & 0x01) * 16) |
08005542: ubfx r1, r0, #10, #1
132 GPIOC->BSRR = (ILI9341_PIN_D4 << 16) >> (((data >> 4) & 0x01) * 16) |
08005546: asr.w r2, lr, r2
134 (ILI9341_PIN_D10 << 16) >> (((data >> 10) & 0x01) * 16) |
0800554a: lsls r1, r1, #4
0800554c: asr.w r1, r12, r1
08005550: orrs r2, r5
127 (ILI9341_PIN_D6 << 16) >> (((data >> 6) & 0x01) * 16) |
08005552: ubfx r6, r0, #6, #1
133 (ILI9341_PIN_D9 << 16) >> (((data >> 9) & 0x01) * 16) |
08005556: orrs r2, r1
137 GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
08005558: ubfx r1, r0, #8, #1
127 (ILI9341_PIN_D6 << 16) >> (((data >> 6) & 0x01) * 16) |
0800555c: mov.w r4, #1048576 ; 0x100000
137 GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
08005560: lsls r1, r1, #4
08005562: lsls r6, r6, #4
08005564: asr.w r6, r4, r6
128 (ILI9341_PIN_D13 << 16) >> (((data >> 13) & 0x01) * 16) |
08005568: ubfx r8, r0, #13, #1
137 GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
0800556c: asrs r4, r1
140 GPIOE->BSRR = (ILI9341_PIN_D1 << 16) >> (((data >> 1) & 0x01) * 16) |
0800556e: ubfx r1, r0, #1, #1
122 GPIOA->BSRR = (ILI9341_PIN_D5 << 16) >> (((data >> 5) & 0x01) * 16) |
08005572: ubfx r7, r0, #5, #1
128 (ILI9341_PIN_D13 << 16) >> (((data >> 13) & 0x01) * 16) |
08005576: mov.w r9, #536870912 ; 0x20000000
123 (ILI9341_PIN_D11 << 16) >> (((data >> 11) & 0x01) * 16);
0800557a: ubfx lr, r0, #11, #1
128 (ILI9341_PIN_D13 << 16) >> (((data >> 13) & 0x01) * 16) |
0800557e: mov.w r8, r8, lsl #4
140 GPIOE->BSRR = (ILI9341_PIN_D1 << 16) >> (((data >> 1) & 0x01) * 16) |
08005582: lsls r1, r1, #4
128 (ILI9341_PIN_D13 << 16) >> (((data >> 13) & 0x01) * 16) |
08005584: asr.w r8, r9, r8
140 GPIOE->BSRR = (ILI9341_PIN_D1 << 16) >> (((data >> 1) & 0x01) * 16) |
08005588: asr.w r1, r12, r1
122 GPIOA->BSRR = (ILI9341_PIN_D5 << 16) >> (((data >> 5) & 0x01) * 16) |
0800558c: mov.w r9, r7, lsl #4
123 (ILI9341_PIN_D11 << 16) >> (((data >> 11) & 0x01) * 16);
08005590: mov.w r12, #16777216 ; 0x1000000
08005594: mov.w lr, lr, lsl #4
122 GPIOA->BSRR = (ILI9341_PIN_D5 << 16) >> (((data >> 5) & 0x01) * 16) |
08005598: mov.w r7, #65536 ; 0x10000
123 (ILI9341_PIN_D11 << 16) >> (((data >> 11) & 0x01) * 16);
0800559c: asr.w lr, r12, lr
080055a0: orrs r3, r6
122 GPIOA->BSRR = (ILI9341_PIN_D5 << 16) >> (((data >> 5) & 0x01) * 16) |
080055a2: asr.w r7, r7, r9
129 (ILI9341_PIN_D14 << 16) >> (((data >> 14) & 0x01) * 16) |
080055a6: ubfx r6, r0, #14, #1
080055aa: orr.w r7, r7, lr
080055ae: mov.w r5, #1073741824 ; 0x40000000
080055b2: ldr.w lr, [pc, #120] ; 0x800562c <ili9341_Write+296>
080055b6: lsls r6, r6, #4
080055b8: asr.w r6, r5, r6
135 (ILI9341_PIN_D12 << 16) >> (((data >> 12) & 0x01) * 16);
080055bc: ubfx r5, r0, #12, #1
122 GPIOA->BSRR = (ILI9341_PIN_D5 << 16) >> (((data >> 5) & 0x01) * 16) |
080055c0: str.w r7, [lr, #24]
129 (ILI9341_PIN_D14 << 16) >> (((data >> 14) & 0x01) * 16) |
080055c4: orr.w r3, r3, r8
135 (ILI9341_PIN_D12 << 16) >> (((data >> 12) & 0x01) * 16);
080055c8: mov.w r7, #8388608 ; 0x800000
080055cc: lsls r5, r5, #4
138 (ILI9341_PIN_D7 << 16) >> (((data >> 7) & 0x01) * 16);
080055ce: ubfx r8, r0, #7, #1
141 (ILI9341_PIN_D2 << 16) >> (((data >> 2) & 0x01) * 16);
080055d2: ubfx r0, r0, #2, #1
135 (ILI9341_PIN_D12 << 16) >> (((data >> 12) & 0x01) * 16);
080055d6: asr.w lr, r7, r5
129 (ILI9341_PIN_D14 << 16) >> (((data >> 14) & 0x01) * 16) |
080055da: orrs r6, r3
080055dc: mov.w r5, #33554432 ; 0x2000000
125 GPIOB->BSRR = (ILI9341_PIN_D3 << 16) >> (((data >> 3) & 0x01) * 16) |
080055e0: ldr r3, [pc, #60] ; (0x8005620 <ili9341_Write+284>)
141 (ILI9341_PIN_D2 << 16) >> (((data >> 2) & 0x01) * 16);
080055e2: lsls r0, r0, #4
080055e4: asr.w r0, r5, r0
138 (ILI9341_PIN_D7 << 16) >> (((data >> 7) & 0x01) * 16);
080055e8: mov.w r8, r8, lsl #4
132 GPIOC->BSRR = (ILI9341_PIN_D4 << 16) >> (((data >> 4) & 0x01) * 16) |
080055ec: add.w r5, r5, #1040187392 ; 0x3e000000
125 GPIOB->BSRR = (ILI9341_PIN_D3 << 16) >> (((data >> 3) & 0x01) * 16) |
080055f0: str r6, [r3, #24]
138 (ILI9341_PIN_D7 << 16) >> (((data >> 7) & 0x01) * 16);
080055f2: asr.w r8, r7, r8
132 GPIOC->BSRR = (ILI9341_PIN_D4 << 16) >> (((data >> 4) & 0x01) * 16) |
080055f6: add.w r5, r5, #133120 ; 0x20800
137 GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
080055fa: ldr r7, [pc, #40] ; (0x8005624 <ili9341_Write+288>)
140 GPIOE->BSRR = (ILI9341_PIN_D1 << 16) >> (((data >> 1) & 0x01) * 16) |
080055fc: ldr r6, [pc, #40] ; (0x8005628 <ili9341_Write+292>)
134 (ILI9341_PIN_D10 << 16) >> (((data >> 10) & 0x01) * 16) |
080055fe: orr.w r2, r2, lr
08005602: orrs r1, r0
137 GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
08005604: orr.w r4, r4, r8
196 ILI9341_PORT_WR->BSRR = (ILI9341_PIN_WR << 16)
08005608: mov.w lr, #16777472 ; 0x1000100
132 GPIOC->BSRR = (ILI9341_PIN_D4 << 16) >> (((data >> 4) & 0x01) * 16) |
0800560c: str r2, [r5, #24]
200 }
0800560e: movs r0, #1
137 GPIOD->BSRR = (ILI9341_PIN_D8 << 16) >> (((data >> 8) & 0x01) * 16) |
08005610: str r4, [r7, #24]
140 GPIOE->BSRR = (ILI9341_PIN_D1 << 16) >> (((data >> 1) & 0x01) * 16) |
08005612: str r1, [r6, #24]
194 ILI9341_PORT_WR->BSRR = (ILI9341_PIN_WR << 16)
08005614: str.w r12, [r3, #24]
196 ILI9341_PORT_WR->BSRR = (ILI9341_PIN_WR << 16)
08005618: str.w lr, [r3, #24]
200 }