cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO Pins(Nucleo-H753zi)

Kishen31
Associate

Hello,


I’m working on a project with the NUCLEO-H753ZI board and need to connect multiple devices. I’d like to know:


1. How many GPIO pins are 5 V-tolerant for digital input?
2. How many GPIO pins are available for general use, both 3.3 V-only and 5 V-tolerant, considering the board’s default peripherals?


I want to make sure I safely use the MCU’s GPIOs for my inputs and outputs. Any guidance or reference resources would be appreciated.

Thank You!

2 REPLIES 2
mfgkw
Senior III

In DS12117 taken from https://www.st.com/resource/en/datasheet/stm32h753zi.pdf you find a table 8 "Pin/ball definition" (starting on page 64). Pins marked as "FT" are 5V tolerant as given in table 7.

 

HTH Klaus

TDK
Super User

See also the schematic for the board. Most pins are 5V tolerant.

https://www.st.com/resource/en/schematic_pack/mb1364-h753zi-e01-schematic.pdf

I suggest approaching this the other way--decide how many 5V tolerant pins you need then find a board that supports that. If you need 40-50 or less, you should have no problem.

If you feel a post has answered your question, please click "Accept as Solution".