2023-08-30 3:39 AM
Hello i two questions ,
1) i use mcu STM32F042T6Y a give the same power supply 3.3v to pin VDD,VDDA and VDDIO2, is this a problem?(many gpio(i chose the gipo tollerant) input of mcu work to 5V and i use the usb host of mcu )
2) i want use a external oscillator ASE-8000MHzLCT i connected the oscillator output to PFO and PF1 is flating (not connect),is this corret ? if yes , the oscillator external give me greater stability of interal rc clock ? (i sue mcu as usb host virtual com port)
Solved! Go to Solution.
2023-08-30 3:42 AM - edited 2023-08-30 3:46 AM
Hello @Fabrizio70 ,
1)
You should also respect the the maximum allowed injected current values.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-30 3:42 AM - edited 2023-08-30 3:46 AM
Hello @Fabrizio70 ,
1)
You should also respect the the maximum allowed injected current values.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-30 6:33 AM
I have VD VDDA Vddio2 are same voltage so i think that have respect table 18.
For input voltage i have 5v on the gpio FT so if i understand the maxim volge on FT pin is VDDIO2+4=3,3+4=7 V (I DONT HAVE INTERNALL pull-up/pull-down)
For the the maximum allowed injected current values i dont understand the table 19 my conditon is this :
VIN =5 VDDIO2 =3,3 V so i have VIN > VDIDDO2 ( positive injection)
the table 19 if i understand give me a current positive injextion 0 mA , seem that dont have problem VIN =5V , it is right or i must use voltage traslator ?
thank yuo