cancel
Showing results for 
Search instead for 
Did you mean: 

ATM90E26_STM32G491RE_SPI Unable to read current values

sireevenkat1
Senior

Hello,

I am trying to read voltage, current and frequency from ATM90E26 IC using STM32G491 with SPI communication. I am getting voltage values correctly.

1.But while reading frequency value If I give 100 Hz I am receiving 50 Hz.
2.While reading current values I am getting always zero value.

3.While reading Metering Status register I am getting Meter Status as:E400 or 2400 but From Hardware side its configures as L line mode but from Metering Status register I am getting anti-tampering mode (larger power)
with N line. Is it effecting the current measurement?
4. I am reading Irms register value(L line mode) for current measurement. I am always getting zero value.If I read Irms2(N line current rms) I am getting some value other than zero and its not changing If I change input current also.
5. I read Status register I got E001 value.
6.check sum error means what do I need to do to solve the error?

Can anyone please suggest me how to solve the issues.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

It feels like this is more of a ATM90E26 usage question, not STM32. Perhaps look at some example code and use that as a basis.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

It feels like this is more of a ATM90E26 usage question, not STM32. Perhaps look at some example code and use that as a basis.

If you feel a post has answered your question, please click "Accept as Solution".