cancel
Showing results for 
Search instead for 
Did you mean: 

Question about an online workshop

JCC
Associate

In the "In-Sensor Data Processing: MEMS with ISPU Core"  workshop, could i use NUCLEO-F446RE instead of NUCLEO-L476RG?

4 REPLIES 4
Peter BENSCH
ST Employee

Welcome @JCC, to the community!

To successfully participate in the workshop, you will need a NUCLEO-L476RG, as can be found on the workshop website, because the software examples are tailored to it. After the workshop, you could also use a smaller target MCU such as the STM32F446, even if it is not an ultra-low power MCU and which also only has 512KB flash (L476RG = 1MB).

If you have successfully registered to the workshop, you will receive a cupon code with which you can also order a NUCLEO-L476RG with free shipping in the estore.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JCC
Associate

@Peter BENSCH I ask because there is no stock on the ST store page, could I use another one? 

farnell has some 300...

https://de.farnell.com/stmicroelectronics/nucleo-l476rg/entwicklungsboard-arduino-mbed/dp/2493816

digikey 200...

https://www.digikey.de/de/products/detail/stmicroelectronics/NUCLEO-L476RG/5347711

AScha3_0-1700165250946.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Hello @JCC 

You Can fin this board available on the ST E-store as you Can see here :

Screenshot_2023-11-16-21-12-13-23_40deb401b9ffe8e1df2f1cc5ba480b12.jpg

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.