2023-11-16 12:21 AM
In the "In-Sensor Data Processing: MEMS with ISPU Core" workshop, could i use NUCLEO-F446RE instead of NUCLEO-L476RG?
2023-11-16 1:36 AM - edited 2023-11-16 1:38 AM
Welcome @JCC, to the community!
To successfully participate in the workshop, you will need a NUCLEO-L476RG, as can be found on the workshop website, because the software examples are tailored to it. After the workshop, you could also use a smaller target MCU such as the STM32F446, even if it is not an ultra-low power MCU and which also only has 512KB flash (L476RG = 1MB).
If you have successfully registered to the workshop, you will receive a cupon code with which you can also order a NUCLEO-L476RG with free shipping in the estore.
Does it answer your question?
Regards
/Peter
2023-11-16 11:50 AM
@Peter BENSCH I ask because there is no stock on the ST store page, could I use another one?
2023-11-16 12:07 PM
farnell has some 300...
https://de.farnell.com/stmicroelectronics/nucleo-l476rg/entwicklungsboard-arduino-mbed/dp/2493816
digikey 200...
https://www.digikey.de/de/products/detail/stmicroelectronics/NUCLEO-L476RG/5347711
2023-11-16 12:13 PM