2021-01-18 01:28 AM
Hi,
Hope everybody is doing great !
I am trying to have quectel M66 2G modem running along with our application running on L476RG.
I found the celluar package from ST for B96 modem and could integrate it to our application and it has all the features we need for our project.
I could get it work with M66 upto sim init. but when I try to register to a network with valid apn details, the ATcommand AT+QICSGP is throwning error. I understood that this AT command does different thing for BG96, I tried AT+QIREGAPP for M66, even this is giving error.
Could anyone please give me hints on this.
Best Regards,
Ankush Nagaraju